This pragma is applied to variables that should not be implicitly initialized.
Syntax:
{attribute 'no_init'}
{attribute 'no-init'}
{attribute 'noinit'}
Insertion position: line above the declaration line of the variables concerned in the declaration part.
Example
PROGRAM PLC_PRG VAR A : INT; {attribute 'no_init'} B : INT; END_VAR
When the associated application is reset, the integer variable A
is implicitly re-initialized with 0
, whereas the variable B
retains its current value.