The pragma is used for function blocks that are derived from a function block implemented in SFC and use the fundamental SFC sequence of this base class. The actions called from it exhibit the same virtual behavior as methods. This means that the implementations of the actions in the base class can be replaced by the derived class with its own specific implementations.
If you apply the pragma to the base class, then its actions are protected against overloading.
Syntax:
{attribute 'no_virtual_actions'}
Insert location: Top line in the declaration part of the function block
Example
The function block POU_SFC
is the base class for the derived function block POU_child
. The derived class POU_child
calls the sequence of the base class written in SFC with the special variable SUPER
.


The exemplary implementation of this sequence is limited to the initial step, followed
by a single step with a linked step action ActiveAction
. This step with a linked step action takes care of the configuration of the output
variables.
an_int:=an_int+1; // Counting the action calls test_act:='father_action'; METH(); // Call of the method METH in order to set the string variable test_meth
In the case of the derived class POU_child
the step action is replaced by a special implementation of ActiveAction
. Active Action
differs from the original only by the assignment of the string 'child_action'
in place of 'father_action'
at the variable test_act
.
Likewise, the method METH
, which assigns the string 'father_method'
to the variable test_meth
in the base class, is overwritten so that test_meth
now gets the value 'child_method'
. The main program PLC_PRG
calls an instance of the function block POU_child
, named Child
. As expected, the value of the strings reflects the call of the action and method
of the derived class:

Now, however, you place the pragma {attribute 'no_virtual_actions'}
in front of the base class:
{attribute 'no_virtual_actions'} FUNCTION_BLOCK POU_SFC...
This changes the behavior: While the implementation of the derived class is still
used for the method METH
, the call of the step action now results in a call of the action ActiveAction
of the base class. Therefore test_act
is now given the value 'father_action'
: