You can use this pragma to prevent the instance of a function block from being stored in the retain memory.
Syntax:
{attribute 'no_instance_in_retain'}
Insert location:
Lines above the FUNCTION_BLOCK declaration in the declaration part of the function block.
Now when you declare an instance declaration of the function block as a RETAIN variable, an error message is issued.
See also