The effect of this pragma is that a variable of the type STRING or WSTRING, which is declared in a library function block with this pragma, is initialized when
used in the project with the current namespace of the library.
Syntax
{attribute 'init_namespace'}
Insertion position: the line above the line with the declaration of the variables in a library function block.
Example
The function block “POU” is provided with the necessary attributes:
FUNCTION_BLOCK POU
VAR_OUTPUT
{attribute 'init_namespace'}
myStr: STRING;
END_VAR
An instance fb of the function block POU is defined within the main program PLC_PRG:
PROGRAM PLC_PRG VAR fb:POU; newString: STRING; END_VAR newString := fb.myStr;
The variable myStr is initialized with the current namespace, for example MyLib. This value is assigned to newString in the main program.
See also