NOTICE

VAR_INPUT
declarations in functions or methods that use the attribute lead to compile errors.
Reason: Input variables are unknown in this case at the time of the call, which occurs
implicitly during the online change.
The effect of this pragma is that all functions and programs containing this attribute
are called after an online change. You define the order of calling by means of the
attribute <slot>
.
Syntax:
{attribute 'call_after_online_change_slot' := '<slot>'}
<slot>
: Integer value that defines the ranking in the order of the calls; the lower the
value, the earlier the call takes place. If several function blocks have the same
ranking for the attribute, then the order of their calls remains indefinite.
Call: First line above the declaration part of functions and programs.
If a method possesses the attribute, then CODESYS determines all instances of the function block concerned. CODESYS calls all instances in the specified slot. In this case you have no influence on the order of the instances among themselves.




NOTICE

Since the application cannot run during the online change, each code executed in this situation can lead to a jitter. Therefore, keep the extent of the executive code as small as possible.
See also