This IEC operator is used for bitwise shift of an operand to the right.
erg := SHR (in, n)
in: Operand that is shifted to the right
n: Number of bits for shifting in to the right




NOTICE

If n overwrites the data type width, then it depends on the target system how the BYTE, WORD, DWORD, and LWORD operands are padded. The target systems cause padding with zeros or n MOD <tab width>.
Examples
ST:
PROGRAM shr_st VAR in_byte : BYTE:=16#45; (* 2#01000101 ) in_word : WORD:=16#0045; (* 2#0000000001000101 ) erg_byte : BYTE; erg_word : WORD; n: BYTE :=2; END_VAR erg_byte := SHR(in_byte,n); (* Result is 16#11, 2#00010001 *) erg_word := SHR(in_word,n); (* Result is 16#0011, 2#0000000000010001 *)
FBD: