This IEC operator is used for bitwise shift of an operand to the left.
erg := SHL (in, n)
in: Operand that is shifted to the left
n: Number of bits to shift in to the left




NOTICE

If n overwrites the data type width, then it depends on the target system how the BYTE, WORD, DWORD, and LWORD operands are padded. The target systems cause padding with zeros or n MOD <tab width>.




NOTICE

Please note the number of bits that CODESYS uses for this operation as defined by the data type of the input variable in.
Examples
The results for erg_byte and erg_word are different, although the values of the in_byte and in_word input variables are the same and the data types of the input variables are different.
ST:
PROGRAM shl_st VAR in_byte : BYTE := 16#45; (* 2#01000101 ) in_word : WORD := 16#0045; (* 2#0000000001000101 ) erg_byte : BYTE; erg_word : WORD; n: BYTE := 2; END_VAR erg_byte := SHL(in_byte,n); (* Result is 16#14, 2#00010100 *) erg_word := SHL(in_word,n); (* Result is 16#0114, 2#0000000100010100 *)
FBD: