The IEC operator is used for bitwise selection.
OUT := SEL(G, IN0, IN1) means:
OUT := IN0; if G = FALSE
OUT := IN1; if G = TRUE
Permitted data types:
IN0, ..., INn and OUT: Any identical data type. Make sure that variables of the identical type are used
at all three positions, especially when using user-defined data types. The compiler
checks for type identity and returns any compile errors. The assignment of function
block instances to interface variables is specifically not supported.
G: BOOL




NOTICE

When G is TRUE, CODESYS does not compute an expression that precedes IN0.When G is FALSE, CODESYS does not compute an expression that precedes IN1.
Caution: In the case of graphical programming languages, the expressions at IN0 and IN1 are computed independently of the G input when a “Box”, “Jump”, “Return”, “Line Branch”, or “Edge Detection” precedes.
Examples
ST:
Var1 := SEL(TRUE,3,4); (* Result: 4 *)
FBD: