This IEC operator is used for bitwise rotation of an operand to the left.
Permitted data types: BYTE, WORD, DWORD, LWORD
erg := ROL (in, n)
CODESYS moves in n-times one bit to the left and adds the bit to the leftmost position from the right.




NOTICE

Please note the number of bits that CODESYS uses for this operation as defined by the data type of the input variable in. If this is a constant, then CODESYS uses the smallest possible data type. The data type of the output variables still
does not influence this operation.
Examples
The results for erg_byte and erg_word are different depending on the data type of the input variables, although the values
of the in_byte and in_word input variables are the same.
ST:
PROGRAM rol_st VAR in_byte : BYTE := 16#45; in_word : WORD := 16#45; erg_byte : BYTE; erg_word : WORD; n: BYTE := 2; END_VAR erg_byte := ROL(in_byte,n); (* Result: 16#15 *) erg_word := ROL(in_word,n); (* Result: 16#0114 *)
FBD:

IL: