This operator is an extension of the IEC 61131-3 standard.
At runtime, the operator executes a type conversion of an interface reference into
another type. The operator returns a BOOL result. TRUE means that CODESYS has performed the conversion successfully.
__QUERYINTERFACE(<ITF_Source>,<ITF_Dest>);
1.Operand: Interface reference or FB interface
2.Operand: Interface reference with required target type
The requirement for the explicit conversion is that both the ITF_Source and ITF_Dest
are derived from Interface __System.IQueryInterface. This interface is implicitly available does not require a library.
Example
INTERFACE ItfBase EXTENDS __System.IQueryInterface
METHOD mbase : BOOL
END_METHOD
INTERFACE ItfDerived1 EXTENDS ItfBase
METHOD mderived1 : BOOL
END_METHOD
INTERFACE ItfDerived2 EXTENDS ItfBase
METHOD mderived2 : BOOL
END_METHOD
FUNCTION_BLOCK FB1 IMPLEMENTS ItfDerived1
METHOD mbase : BOOL
mbase := TRUE;
END_METHOD
METHOD mderived1 : BOOL
mderived1 := TRUE;
END_METHOD
END_FUNCTION_BLOCK
FUNCTION_BLOCK FB2 IMPLEMENTS ItfDerived2
METHOD mbase : BOOL
mbase := FALSE;
END_METHOD
METHOD mderived2 : BOOL
mderived2 := TRUE;
END_METHOD
END_FUNCTION_BLOCK
PROGRAMM POU
VAR
inst1 : FB1;
inst2 : FB2;
itfbase1 : ItfBase := inst1;
itfbase2 : ItfBase := inst2;
itfderived1 : ItfDerived1 := 0;
itfderived2 : ItfDerived2 := 0;
xResult1, xResult2, xResult3, xResult4: BOOL;
END_VAR
xResult1 := __QUERYINTERFACE(itfbase1, itfderived1); // xResult = TRUE, itfderivedi1 <>0
// references the instance inst1
xResult2 := __QUERYINTERFACE(itfbase1, itfderived2); // xResult = FALSE, itfderived2 = 0
xResult3 := __QUERYINTERFACE(itfbase2, itfderived1); // xResult = FALSE, itfderived1 = 0
xResult4 := __QUERYINTERFACE(itfbase2, itfderived2); // xResult = TRUE, itfderived2 <> 0
// references the instance inst2