The operator is an extension of the IEC 61131-1 standard.
At runtime, the operator yields the position of a variable in the declaration part
or in the implementation part of a POU. The operator has to be assigned the variables
of type STRING in the declaration part or in the implementation part.
Result of __POSITION
-
Declaration part:
'Line <line number> (Decl)' -
Implementation part:
'Line <line number>, Column <column number> (Impl)'
Example
PROGRAM PROG1 VAR strPOS : STRING := __POSITION(); //Yields the line number of this declaration strlocalPOS : STRING; END_VAR strlocalPOS := __POSITION(); //Yields the line and column number of this assignment