This IEC operator is used for the bitwise OR of bit operands. 
When at least one of the input bits yields 1, the output bit also yields 1; otherwise 0.
Permitted data types: BOOL, BYTE, WORD, DWORD, LWORD
Examples
Result in Var1 ist 2#1001_1011
ST:
Var1 := 2#1001_0011 OR 2#1000_1010;
FBD: