This IEC operator is used for assigning a variable to another variable of a corresponding type.
Because the MOVE block is available in the CFC, FBD, and LD editors, you can also use the EN/ENO functionality
for variable assignment.
CFC with EN/ENO function:
CODESYS assigns the value of var1 to var2 only if "en_i" yields TRUE.

ST:
ivar2 := MOVE(ivar1);
This corresponds to:
ivar2 := ivar1;