This IEC operator is used for the minimum function. It yields the smallest value of two values.
‎OUT := MIN(IN0,IN1)‎
Permitted data types: all
Examples
Result: ‎30‎
ST:
Var1:=MIN(90,30); Var1 := MIN(MIN(90,30),40);
FBD:

This IEC operator is used for the minimum function. It yields the smallest value of two values.
‎OUT := MIN(IN0,IN1)‎
Permitted data types: all
Examples
Result: ‎30‎
ST:
Var1:=MIN(90,30); Var1 := MIN(MIN(90,30),40);
FBD: