This IEC operator is used for the maximum function. It yields the largest value of two values.
OUT := MAX(IN0, IN1)
Permitted data types: all
Examples
ST:
Result: 90
Var1 := MAX(30,40); Var1 := MAX(40,MAX(90,30));
FBD:
Result: 90

This IEC operator is used for the maximum function. It yields the largest value of two values.
OUT := MAX(IN0, IN1)
Permitted data types: all
Examples
ST:
Result: 90
Var1 := MAX(30,40); Var1 := MAX(40,MAX(90,30));
FBD:
Result: 90