This IEC operator is used for the "less than" function.
Permitted data types of the operands: any basic data type.
If the first operand is less than the second operand, then the operator yields the
result TRUE; otherwise FALSE.
Examples
Result: TRUE
ST:
Var1 := 20 < 30;