This IEC operator is used for the "less than or equal to" function.
Permitted data types of the operands: any basic data type.
If the first operand is less than or equal to the second operand, then the operator
                     yields the result TRUE; otherwise FALSE.
Examples
Result in Var1: TRUE
ST:
Var1 := 20 <= 30;