Functions for preventing division by zero: CheckDivInt, CheckDivLint, CheckDivReal, and CheckDivLReal 
To prevent division by zero, you can use the functions CheckDivInt, CheckDivLint, CheckDivReal, and CheckDivLReal. If you include these functions in the application, then they are called before each
                     division operation in the code.




CAUTION

To obtain the feature for monitoring functions, do not edit the declaration section. However, you are permitted to add local variables.
The default implementation of CheckDivReal:
Declaration section:
// This is automatically generated code: DO NOT EDIT FUNCTION CheckDivReal : REAL VAR_INPUT divisor:REAL; END_VAR
Implementation section:
// This automatically generated code is a suggested implementation. IF divisor = 0 THEN CheckDivReal:=1; ELSE CheckDivReal:=divisor; END_IF;
The DIV  operator uses the output of the CheckDivReal function as a divisor. In the sample program below, CheckDivReal prevents division by 0 by changing the implicit value of the divisor d from "0" to 1 before the division operation is executed. Therefore, the division result is 799. 
PROGRAM PLC_PRG VAR erg:REAL; v1:REAL:=799; d:REAL:=0; END_VAR erg:= v1 / d;
See also