Symbol: 
A global variable list (task-local) is used for the declaration, editing and display of global variables. For this special global variable list, the declared variables in the list can be written by one task only. All other tasks have only read-only access. This makes sure that the values of these variables are always consistent, even for multicore projects.
The object is available for compiler version 3.5.13.0 with the corresponding device description.
| “Task with write access” | Task that has exclusive write access to the variables. |