Symbol: 
The object is used as a node for data sources below it. At least one data source has to exist. An application with the data source manager communicates with remote devices.
See also
Command 'Add Object' > 'Data Source'
Function: The command opens the “Add Data Source” dialog.
Call
-
Menu bar: “Project”
-
Context menu in the “Devices” view of the CODESYSperspective
-
Context menu in the “Data Sources” view of the “HMI” perspective
Requirement: The “Data Source Manager” object is selected that should have an additional data source.
Dialog 'Add Data Source'
|
“Name” |
Example: |
|
“Select data source type” |
Data source type that matches the controller configuration in order to establish communication.
|
|
“Add” |
Opens the “Initialize Data Source - Provider settings” dialog. The contents of the dialog depend on the selected data source type. |




NOTICE

The remote PLC should be running and the remote PLC application loaded and started.
Dialog 'Initialize Data Source Wizard - Provider settings' (for 'CODESYS Symbolic')
The settings of this dialog are described in the following chapter: Object 'Data Source' - Tab 'Communication".
The dialog is used to configure the connection initially when you have selected “CODESYS Symbolic” as the data source type. The communication is done by means of symbolic monitoring. The configuration can be modified later in the editor of the data source on the “Communication” tab.
Dialog 'Initialize Data Source Wizard - Provider settings' (for 'CODESYS ApplicationV3')
The settings of this dialog are described in the following chapter: Object 'Data Source' - Tab 'Communication".
The dialog is used to configure the connection initially when you have selected “CODESYS ApplicationV3” as the data source type. The communication is done by means of address monitoring.
Dialog 'Initialize Data Source Wizard - Provider settings' (for 'OPC UA Server')
The settings of this dialog are described in the following chapter: Object 'Data Source' - Tab 'Communication".
The dialog is used to configure the connection initially when you have selected “OPC UA Server” as the data source type. The communication takes place over a TCP connection.
Dialog 'Initialize Data Source Wizard - Browse data items'
The settings of this dialog are described in the following chapter: Object 'Data Source' - Dialog 'Choose Variables'.
Function: You can select the variables for data transmission from the variables of the remote PLC. By clicking “Finish”, the data source is initialized and the data types and variables (data interface) are declared below the folder “DataSources_Objects”. You can modify the settings in the editor of the data source object.
Call: Automatic
See also