In this tab of the generic device editor, you define the access rights of different user groups (clients) to the individual symbol sets available on the controller.
Requirement: User management must be set up on the PLC. An application was downloaded to the controller for which symbol sets were defined in the CODESYS project. They have access data for logging in to the controller.
In the “Symbol Sets” view, all symbol sets are listed below the “Application” node whose definition was downloaded with the application to the controller.
In the “Rights” view, the user groups defined in the user management of the controller are listed
in a table. When a symbol set is selected, you see the access rights of the corresponding
user group to the symbols of this set.
: Access granted;
: Access not granted. You can change the access rights by double-clicking the symbol.
Click the
button to save the current access configuration to an XML file The file type is “Device symbol management files (*.dsm)”. Click the
button to read a file like this from the hard drive.