You have added a “Data Source Manager” object and below it a “Data Source” object below your application in the device tree. The connection parameters are displayed in the data source editor of the “Communication” tab. You can modify it there.
The data source type and the current connection type are listed in the status bar. It is not possible to modify the data source type later.