Symbol: 
Function: The dialog includes the trace configuration for the data recording.
Call
- 
                           
“Trace Configuration”; context menu
 - 
                           
Link “Configuration” in the trace editor
 - 
                           
Link “Add Variable” in the trace editor
 
Requirement: The editor of a trace object is open and active.
Tree view 'Trace Record'
The tree view lists the variables that are traced and allows for access to the variable settings.
| 
                                  Selected trace name  | 
                              
                                  The “Record Settings” subdialog is displayed on the right.  | 
                           
| 
                                  Selected trace variable  | 
                              
                                  The “Variable Settings” subdialog is displayed on the right.  | 
                           
| 
                                  
  | 
                              
                                  Adds a new trace variable. The “Variable Settings” subdialog opens on the right and it is partially configured. Select a variable in the input field of the “Variable” setting to trace its value curve.  | 
                           
| 
                                  “Assign to Diagram”  | 
                              
                                  Lists the diagrams (in the submenu on the right) where the selected variable is not currently displayed. Select a diagram to display the variable there. The command is available when a variable is selected in the tree view. Hint: When the command is deactivated, the variable is already displayed in all diagrams.  | 
                           
| 
                                  “Enabled”  | 
                              
                                  Selected by default Disabled variables are displayed as disabled. They are neither displayed nor recorded.  | 
                           
Tree view 'Presentation (Diagrams)'
The tree view lists the diagrams that are displayed in the trace editor and allows for access to their display mode.
| 
                                  Selected node “Time axis”  | 
                              
                                  The “Display Mode” subdialog for the time axis is displayed on the right. You can specify the time axis display. See below.  | 
                           
| 
                                  Selected diagram name  | 
                              
                                  The settings for the coordinate system of the diagram and a preview are displayed on the right. See below.  | 
                           
| 
                                  Selected node “Y-axis”  | 
                              
                                  The “Display Mode” subdialog is displayed on the right. You can specify the axis display. See below.  | 
                           
| 
                                  “Show variables”  | 
                              |
| 
                                  Selected trace variable  | 
                              
                                  The “Variable Settings” subdialog is displayed on the right. You can configure the trace variable. See below. Note: These are the same settings that can be accessed in the “Trace Record” tree view.  | 
                           
| 
                                  
  | 
                              
                                  Adds a new diagram below and displays it in the tree view “Presentation (Diagrams)”.  | 
                           
| 
                                  
  | 
                              
                                  Adds a new trace variable. The “Variable Settings” subdialog opens on the right and it is partially configured. Select a variable in the input field of the “Variable” setting to trace its value curve. Specify its display. In addition, the variable is assigned to the selected diagram.  | 
                           
| 
                                  “Add Existing Variable”  | 
                              
                                  Lists all trace variables (in the submenu on the right) where the selected diagram is not currently displayed. Select a variable in order to display it in the selected diagram. Hint: When the command is deactivated, all trace variables are already displayed in the selected diagram.  | 
                           
Subdialog 'Record Settings'
Requirement: The top node is selected in the “Trace Record” tree view.
| 
                                  “Enable trigger”  | 
                              
                                  
 
  | 
                           
| 
                                  “Trigger variable”  | 
                              
                                  Signal that is used as a trigger. A complete instance path is required. A valid trigger signal is an IEC variable, a property, a reference, a pointer, an
                                    array element of the application, or an expression. Allowed types are all IEC-based
                                    types except  When the runtime system uses the   | 
                           
| 
                                  “Trigger parameter”  | 
                              
                                  System parameter that is used as a trigger The “Input Assistant” dialog lists all valid system parameters in the “Parameters” category of the “Categories” tab.  | 
                           
| 
                                  
  | 
                              
                                  Allows the selection of “Trigger variable” or “Trigger parameter”  | 
                           
| 
                                  “Trigger edge”  | 
                              
                                  Defined the edge detection for triggering: 
  | 
                           
| 
                                  “Post trigger (samples)”  | 
                              
                                  Number of records per trace variable that are buffered after triggering. Default:
                                      | 
                           
| 
                                  “Trigger level”  | 
                              
                                  Value that is reached to start the triggering  | 
                           
| 
                                  “Task”  | 
                              
                                  Task in which the data is recorded.  | 
                           
| 
                                  “Recording condition”  | 
                              
                                  At runtime, the application checks the recording condition. If it is fulfilled, then the trace data is buffered. Record condition for data recording with  
 Recording condition for a data recording with IEC code. 
  | 
                           
| 
                                  “Comment”  | 
                              
                                  Comment (for example, from the recording condition)  | 
                           
| 
                                  “Resolution”  | 
                              
                                  Unit of measure for the time stamp that is recorded per data set 
  | 
                           
| 
                                  “Automatic restart”  | 
                              
                                  
  | 
                           
| 
                                  “Advanced”  | 
                              
                                  Opens the “Advanced Trace Settings” dialog.  | 
                           
See also
Subdialog 'Variable Settings'
Requirement: A trace variable is selected in the “Trace Record” or “Display (Diagrams)” tree view.
| 
                                  “Variable”  | 
                              
                                  Valid variable Variable; value recorded with full instance path. Valid: 
 Allowed data type 
 When the runtime system uses the   | 
                           
| 
                                  “Parameter”  | 
                              
                                  Parameter whose data is recorded. Requirement: Runtime system with  The “Input Assistant” dialog lists all valid system parameters in the “Parameters” category of the “Categories” tab.  | 
                           
| 
                                  
  | 
                              
                                  Allows toggling between “Variable” and “Parameter”  | 
                           
| 
                                  “Color”  | 
                              
                                  Color of the variable in the trace diagram  | 
                           
| 
                                  “Line type”  | 
                              
                                  Display as line chart 
  | 
                           
| 
                                  “Point type”  | 
                              
                                  Display as scatter chart 
  | 
                           
| 
                                  “Activate minimum warning”  | 
                              
                                  
  | 
                           
| 
                                  “Critical lower limit”  | 
                              
                                  If the value of the trace variable falls below the limit, the variable is displayed in the warning color.  | 
                           
| 
                                  “Color”  | 
                              
                                  Warning color on falling below the limit  | 
                           
| 
                                  “Activate maximum warning”  | 
                              
                                  
  | 
                           
| 
                                  “Critical upper limit”  | 
                              
                                  If the value of the trace variable exceeds the upper limit, the variable is displayed in the warning color.  | 
                           
| 
                                  “Color”  | 
                              
                                  Warning color on exceeding the limit  | 
                           
Subdialog 'Display Mode'
Requirement: An axis is selected in the tree view “Presentation (Diagrams)”
| 
                                  “Display Mode”  | 
                              
                                  Scaling 
  | 
                           
| 
                                  “Minimum”  | 
                              
                                  Literal, variable (integer data type), or constant variable (integer data type). It contains the initial value of the segment. Requirement: The “Display Mode” is “Fixed”. Examples:  Note: The variable has to have an initial value. This is important for the offline
                                    display and the scaling subdivision. Example:   | 
                           
| 
                                  “Maximum”  | 
                              
                                  Literal, variable (integer data type), or constant variable (integer data type). It contains the end value of the segment. Requirement: The “Display Mode” is “Fixed”. Examples:  Note: The variable has to have an initial value. This is important for the offline
                                    display and the scaling subdivision. Example:   | 
                           
| 
                                  “Length”  | 
                              
                                  Constant segment length; the initial value is adapted automatically.  | 
                           
| 
                                  “Grid”  | 
                              
                                  
  | 
                           
| 
                                  “Fixed spacing”  | 
                              
                                  
  | 
                           
| 
                                  “Distance”  | 
                              
                                  Distance between tick marks  | 
                           
| 
                                  “Subdivisions”  | 
                              
                                  Number of subdivisions between two tick marks  | 
                           
| 
                                  “Font”  | 
                              
                                  Font for the time axis.  | 
                           
| 
                                  Link “Preview”  | 
                              
                                  Displays the preview of the diagram.  | 
                           
Diagram preview
Requirement: A diagram is selected in the tree view “Presentation (Diagrams)”

| 
                                  “Background color”  | 
                              
                                  Background color of the diagram.   | 
                           
| 
                                  “Background color on selection”  | 
                              
                                  Background color of the selected diagram.  | 
                           
| 
                                  Link “Add Variable”  | 
                              
                                  Adds a new trace variable (in the “Trace Record” tree view).  | 
                           
| 
                                  Link “Delete Variable”  | 
                              
                                  Deletes the selected trace variable (in the “Trace Record” tree view).  | 
                           
| 
                                  Link “Add Diagram”  | 
                              
                                  Adds a new diagram (in the “Display” tree view).  | 
                           
| 
                                  Link “Delete Diagram”  | 
                              
                                  Deletes the selected diagram (in the “Display” tree view).  | 
                           
| 
                                  Link “Reset Display Settings”  | 
                              
                                  Resets the display settings of either the selected diagram or Y-axis to the default values.  | 
                           
| 
                                  “OK”  | 
                              
                                  Accepts the configuration changes and saves the trace configuration.  | 
                           
 
: Triggering is enabled. The trace data is buffered at runtime only when a trigger
                                    signal has been sent. You determine how the trigger signal is sent in the 
: Continuous display of current records