Function: The dialog defines the default settings for all POUs used in the project, which are programmed in SFC.
Call: Main menu “View Properties”, context menu of a SFC POU in the view “Device” or “POUs”.
Flag
List of all possible SFC flags |
“Use” “Declare” If “Declare” is activated, but “Use” is not activated, the variable will be declared but the flag has no effect in the program execution. Hint: If you have manually declared a SFC variable you have to disable the declaration of this flag in the “SFC Settings”. Otherwise the automatically generated flag will overwrite the manually declared flag. Hint: A automatically declared flag variable is only visible in the online mode in the declaration part of the SFC editor. |
“Use defaults” |
|
See also
Build
“Calculate active transitions only” |
|