Function: The tab contains options for the monitoring of transitions in SFC.
Call: Select transition object, click “Properties”; menu bar: “View Properties”.
“Enable monitoring” |
|
“Monitoring using call” |
Note: When you activate this option, you have to consider possible side effects. These kinds of side effects can occur if additional operations are implemented in the transition. |