Function: The settings on this tab define when and how a boot application is created from the application.
Requirement: The device supports the settings.
Call: Select the application object; context menu: “Properties”; menu bar: “View Properties”, “Boot Application” category
“Create implicit boot application on download” |
A boot application is created automatically when downloading the application. |
“Create implicit boot application on Online Change” |
A boot application is created automatically when for an online change. |
“Remind boot application on project close” |
Before closing the project, CODESYS prompts to create the boot application. |
“Verify boot application after creation” |
After the boot application is created, an independent service checks whether or not the boot application has been created correctly. |
Regardless of the presets defined here, you are always able to create a boot application explicitly when you login.
See also