Symbol:
Function: The dialog contains settings for the behavior of CODESYS when loading and saving a project.
Call: Menu bar: “Tools Options”, category “Load and Save”
“Create backup files” |
|
“Automatically save every … minutes” |
CODESYS deletes the |
“Save before build” |
CODESYS saves the project automatically before each build operation. |
“Create project recovery information” |
Requirement: The “No protection” option is selected in the project settings in the “Security” category. This means that the project is not protected against unauthorized access and data manipulation, and there is no integrity check when the project is loaded.
Note: The project restore records every change on the hard disk when the change is made. If a power failure or hard disk error occurs on the hard disk during this operation, then the last change may be lost. |
“Advanced Settings” |
The “Advanced Settings” dialog opens. |
“At startup” |
List box for the startup screen of CODESYS:
|
“News page” |
URL that is opened by means of the command “Help CODESYS CODESYS Homepage”. By default, this page is |
“Project compression” |
|
“Level” |
Requirement: The “No protection” option is selected in the project settings in the “Security” category. This means that the project is not protected against unauthorized access and data manipulation, and there is no integrity check when the project is loaded. List box for the compression level that is used when saving the project.
|
“Load Behavior” |
|
|
Libraries and compilation information are loaded in the background while you edit the project. |
See also