Function: The dialog allows for the transfer of CODESYS options and package installations from an older CODESYS installation that was found in the local computer.
Call: The dialog opens when a recently installed CODESYS version is started for the first time and an older version is installed on the computer.
“Program settings” |
|
“Packages” |
|
“Import” |
The program settings and/or options are transferred to the current CODESYS version. |
“Skip” |
The program settings and/or options are not transferred to the current CODESYS version. |
See also