Function: The dialog defines how references to devices that are no longer available are to be handled.
Call: When opening a CoDeSys V2.3 project in V3, the dialog opens when the converter detects a device reference which cannot be used anymore.
A CoDeSys V2.3 project can be converted into a CODESYS V3 project only if the CODESYS V2.3 Converter package is installed in CODESYS V3. The package is available in the CODESYS Store.
|
“Use the following device that has already been installed” |
CODESYS replaces the previously used device in the device tree with another device. The “Browse” button opens a dialog for selecting from the local device repository. |
|
“Ignore the device. All device specific objects will not be available in the new project” |
The device entry with all objects inserted below it is removed from the device tree. |
|
“Remember this mapping for all future occurrences of that device” |
The settings made here in the dialog are saved in the CODESYS Options, in the “CODESYS V2.3 Converter” category. As a result, they are also valid for future project conversions. |