Function: Use this dialog for generating new toolbars or customizing existing toolbars.
Call: Main menu “Tools Customize” (“Toolbars”).
When you click “OK” to close the dialog, the changes are visible in the menu bar of the CODESYS user interface.
|
Display of currently defined toolbars. In CODESYS, the associated commands are listed below each toolbar in the order they will appear in the toolbar. Double-clicking a toolbar in the list switches to editing mode. |
|
|
“Add Toolbar” |
Enabled when a toolbar is selected. In CODESYS, this adds a toolbar above the selected toolbar and places the cursor in the name field of the new toolbar. |
|
“Add Command” |
Enabled when you select a command or blank command entry below a toolbar. Adds a command above the selected command. Opens the “Add Command” dialog. Use the “Add Command” dialog to select one or more commands. Left part: List of categories. Right part: List of commands in the selected category. |
|
“Add Separator” |
Adds a separator above the selected command. |
|
“Hide” |
Hide the selected toolbar from the user interface. |
|
“Show” |
Shows the selected hidden toolbar in the CODESYS user interface. |
|
“Reset” |
Resets the default settings of the toolbars. |
|
“Load” |
Loads the settings from a stored file (<file name>.opt.tbar). |