Function: This dialog box is used for defining keyboard shortcuts (quick access keys or keyboard combinations) for commands.
Call: Main menu “Tools Customize” (“Keyboard”).
“Shortcuts for selected command” |
Keyboard shortcuts for the selected command The drop-down list can include more than one keyboard shortcut for the command. |
“Press shortcut keys” |
Input field for the keyboard shortcut of the selected field. Permitted combinations include [Ctrl], [Alt], [Shift], and other keys. You clicking “Assign” to assign a recorded keyboard shortcut to a selected command. |
“Shortcut keys currently used by” |
Command assigned to the currently defined keyboard shortcut |
“Reset” |
Resets the default settings of the keyboard shortcuts. |
“Load” |
Loads the settings from a stored file (<file name>.opt.keyb). |