Declaring global variables that are available within the application.
Requirement: A project is open.
- 
                           In the Device tree of your project, select the application in which the global variables are to be valid. 
- 
                           Select the context menu command “Add Object Global Variable List”. CODESYS inserts the “GVL” in the Device tree under the application and opens it in the editor. 
- 
                           Select the menu command “Edit Auto Declare”. The dialog box “Auto Declare” opens. 
- 
                           In the selection list “Scope”, select the entry “VAR_GLOBAL”. 
- 
                           In the field “Name”, enter a name for the global variable. 
- 
                           Select a data type from the selection list “Type”. 
- 
                           If your variable is to have an initialization value other than the standard initialization value, click on  next to the field “Initialization”. next to the field “Initialization”.The dialog box “Initialization Value” opens. 
- 
                           Double-click on the cell “Init value” of your variable and enter the desired valid value. 
- 
                           Click on “OK”. The initialization value is displayed in the dialog box “Auto Declare”. 
- 
                           Activate one of the “Flags” if necessary. 
- 
                           Confirm your entries by clicking on the button “OK”. CODESYS inserts the declared variable in the GVL. The global variable is available in the total application of your project. 
Declaring global variables that are available in the entire project.
- 
                           Select the menu command “View POUs”. The “POUs” view opens. 
- 
                           In the “POUs” view, select the uppermost node with the project name and select the context menu command “Add Object Global Variable List”. CODESYS inserts the “GVL” in the “POUs” view and opens it in the editor. 
- 
                           Select the menu command “Edit Auto Declare”. The dialog box “Auto Declare” opens. 
- 
                           In the selection list “Scope”, select the entry “VAR_GLOBAL”. 
- 
                           In the field “Name”, enter a name for the global variable. 
- 
                           Select a data type from the selection list “Type”. 
- 
                           If your variable is to have an initialization value other than the standard initialization value, enter it in the column “Initialization”. 
- 
                           Activate one of the “Flags” if necessary. 
- 
                           Confirm your entries by clicking on the button “OK”. CODESYS inserts the declared variable in the GVL. The global variable is now available in the entire project. 
See also