Variables with these data types are converted to a platform-compliant data type, depending on the target system.
CODESYS supports systems with address registers of 32-bit and 64-bit widths. For making the
IEC code as independent from the target system as possible, you use the pseudo data
types __UXINT, __XINT, and __XWORD. The compiler checks which target system types are current and then converts these
data types into the appropriate standard data types.
Moreover, type conversion operators are provided for variables of these data types.
|
Type conversion on 64-bit platforms |
Type conversion on 32-bit platforms |
|
|
|
|
|
|
|
|
|
|
|
|
|
See also