Function: This command releases a docked view from its frame in the user interface and repositions it on the screen as a floating window.
Call: Main menu “Window”
Requirement: The application is in online mode.
This window can then be positioned outside of the user interface. Use the “Dock” command to return a floating window to the frame of the user interface.
See also