Symbol:
Function: This command initiates the synchronization of the recipes from the open recipe definition in the project and the recipes located on the device in the form of recipe files.
Call: Menu bar: “Recipes”.
Requirement: The application is in online mode and a recipe definition is open in the editor.
In detail, the synchronization is described as follows:
-
The current values for the recipe variables located in the project are overwritten by the values from the recipes on the controller. As a result, there is likely an online change at the next login.
-
If recipe variables are defined in the recipe files on the controller, and the recipe variables are missing in the recipe definition of the project, then these variables are ignored when at the time of download. Before that, a message appears for each recipe file regarding the variables in question.
-
If recipe variables are missing in the recipe files on the controller, and these recipe variables are included in the recipe definition of the project, then a message appears for each recipe file with the variables in question.
-
If more recipes for these variables have been created on the controller, then they are added to the recipe definition in the project.