Symbol: 
Function: This command opens a macro for editing in the macro editor.
Call: Main menu “SFC”
Requirement: A macro is selected.
By choosing this command, CODESYS closes the main view of the SFC editor and opens the macro editor. This is also an SFC editor for editing the section of the SFC diagram that is displayed as a macro box in the main view.
Click “Zoom Out of Macro” to return to the main view.
See also