Function: This command embeds every step action or transition, which is called by a step or transition in the SFC box, with the caller. In this way, the action or transition object can be called only from exactly this caller (pseudo-embedding). The result is that copying step and transition elements that call cations or transitions automatically creates new action or transition objects. the implementation code is also copied.
Call: Menu bar: “SFC”.
For more details about duplication mode, refer to the help page for the SFC element properties and the instructions for adding step actions.
Pseudo-embedded objects can be hidden in the “Devices” or “POUs” view by means of a command.
See also