Function: This command selects the entire code section within the currently selected code parentheses.
Call: Menu “Edit Extended”
Requirement: A text editor is opened and the cursor is positioned at an opening or closing code parenthesis. If you position the cursor at a code parenthesis, CODESYS displays the corresponding parenthesis in color, provided you have activated the option “Associated parentheses” in the project options in the “Text Editor” category, “Text Area” tab.
See also