Function: This command executes a script that is stored in the ScriptDir
folder.
Call: Menu bar: “Tools Scripting Scripts”.
Requirement: The ScriptDir
folder exists in the CODESYS installation directory. Python scripts are stored in this folder with the file extension
.py
.
All scripts that are contained in the ScriptDir
folder are executable as menu commands and are sorted alphabetically by file name.