Function: The command opens a dialog to reset the device to its factory settings. All applications, boot applications, and remanent variables will be deleted from the device. Depending on the version of the device, a selection of the elements to be deleted can be made in this dialog. When these elements are unselected in the dialog, they are not deleted during the reset and remain on the controller. By default, all elements are selected and everything is deleted. Elements that are not available for selection are generally also deleted.
Call: Right-click a programmable device in the device tree.




NOTICE

If a safety controller is inserted below a controller, then this command can interrupt the communication connections permanently.
Connections of the safety controller to other safety controllers (via safety network variables), to field devices, and to the development system are affected. The safe field devices or other safety controller can enter the safe state as a reaction. The connection to the development system is affected only when a safety controller that is connected to the main controller via a fieldbus.
For more information, see the "Subordinate Safety Controllers" chapter.
After restarting with “Reset Origin Device”, the following happens:
-
All applications are reset as with the “Reset Origin” command.
-
All files, which are not deleted by the “Reset Origin” command, are deleted (for example, files from visualization, alarms, and recipes).
-
The user management is deleted.
-
All certificates which are currently managed by the runtime system are deleted.
|
Note: When resetting the device, the objects selected in this dialog are also deleted. If not all displayed objects are selected in this dialog, then possibly other objects can no longer be used or they are also deleted. . |
|
|
“Delete” |
|
|
“Object” |
Objects that can be excluded from “Delete”. The listed objects depend on the version of the controller. In version 3.5.16.20 and higher, the following objects can be excluded from the delete operation.
|
: The object is deleted when the