Function: The command results in a reset origin of the active application on the controller.
Call: Menu bar: “Online”
Requirement: The application is in online mode.




NOTICE

If a safety controller is inserted below a controller, then this command can interrupt the communication connections permanently.
Connections of the safety controller to other safety controllers (via safety network variables), to field devices, and to the development system are affected. The safe field devices or other safety controller can enter the safe state as a reaction. The connection to the development system is affected only when a safety controller that is connected to the main controller via a fieldbus.
For more information, see the "Subordinate Safety Controllers" chapter.
After restarting with “Reset Origin”, the following happens:
-
The application code is deleted, and as a result the application has no state.
-
Variables are deleted, and the values are lost.
-
Retain variables are deleted, and the values are lost.
-
Persistent variables are deleted, and the values are lost.
-
Breakpoints that were set in the code are lost.