Symbol: 
Function: This command reads the variable values of a recipe from the controller.
Call: Main menu “Recipes”.
Requirement: The application is in online mode and you have selected the value of a recipe in the recipe definition.
When you choose this command, CODESYS overwrites the values of the selected recipe with the read values from the controller.
If you have selected the option “Recipe Management in the PLC”, please note the following.
If you change recipes in the project by choosing the command “Load Recipe” or “Read Recipe”, then an online change is required when logging in again.