Function: This command opens the “Create Localization Template” dialog. Define here which information should be exported from the project to a translation
template (*.pot file).
Call: Menu bar: “Project Project Localization”.
Requirement: A project is open.
Dialog 'Create Localization Template'
This dialog is used for selecting the textual information that should be used in the localization template.
|
“Names” |
Texts, such as dialog captions and object names in the device tree |
|
“Identifier” |
Variable identifier (example: |
|
“ Strings” |
Example: |
|
“Comments” |
Comment texts in the POUs |
|
“Position information” |
Selection of which positions of the selected text categories in the project should be included in the translation file. The position information is located in the first line(s) of a segment for a translation. Example:
|
|
“Generate” |
This button opens the dialog for saving a file. The translation template is created
in a text file of type |
See also
-
Help about CODESYS Visualization: Multi-language capability