Keyboard shortcut: [Shift]+[F6]
Function: This command sets the focus on the previous pane.
Call: Main menu “Window”
Requirement: An object is open that contains two or more panes.
Example: If an object is open in the ST editor and the cursor is currently in the declaration section, then command sets the focus to implementation section.
See also