Symbol:
Function: The command opens the “Package Manager” dialog where you install, uninstall, and manage packages.
Call: Menu bar: “Tools”
You can also call the Package Manager as a standalone application from the command line.
List of installed packages with “Name”, “Version”,“Installation date”, “Update info”, “License info” If a package originates from the CODESYS Store, then CODESYS identifies it with the red package When an update is available, CODESYS indicates this with an entry in the “Update info” column and with the |
|
“Refresh” |
Refreshes the list |
“Install” |
Opens the standard dialog for finding a file in the file system. By default, the file type is *.package. You can also install two versions of a package. After you select the package, the “Check package signatures” dialog opens.
After the package is selected, the installation wizard opens with the dialogs:
When this dialog is successfully completed, the selected package is ready for installation. You have to close all CODESYS instances in order for the package installation to be automatically started and run. |
“Uninstall ” |
Uninstalls the selected package
When this dialog is closed, all CODESYS instances have to be closed in order for the package uninstallation to start. |
“Details” |
Opens the “Details” dialog for the selected package with the following tabs:
|
“Search updates in background” |
|
“Display versions” |
|
You can compare the “Checksum” with the package checksum from the package vendor. CODESYS displays this checksum in the “Details” dialog and in the “Installation - License Agreement” dialog of the installation wizard. You do this to make sure that you have installed an original package.
If you have installed a newer version of the programming system in the same installation directory as the previous version, the license information about the previously installed package remains unchanged and CODESYS displays the information in the “Package Manager” dialog.
“Search Updates” |
Searches for the selected package on your system and in the CODESYS Store Updates. CODESYS displays the found updates in the “Update Info” column of the package list. |
“Download” |
Installs the update package from the “Download Package” dialog. In the “Download Package” dialog, click the “Download and Installation” button for this. |
“Rating” |
Give an rating of the package |
“CODESYS Store” |
Link to the homepage of the Store |