Function: The command opens the “OPC UA Information Model” dialog. The OPC UA information models, which are installed on the local system and can be integrated in CODESYS projects, are managed in the dialog.
Call: Menu bar: “Tools”
|
“Location” |
Displays the OPC UA information model directories on the local system. The list box shows the currently set locations. By default, CODESYS creates the system repository during installation. The information models of the selected location are listed in the “Installed OPC UA information models” area. |
|
“Edit Locations” |
Opens the “Edit Repository Locations” dialog. |
|
“Installed OPC UA information models” |
|
|
List of installed information models. Double-click to open installed information model documentation. Note: The information models of this repository can also be added to project archives. |
|
|
“Install ” |
Opens the “Select Installed OPC UA Information Model(s)” dialog.
|
|
“Uninstall” |
Uninstalls the selected OPC UA information model. When you delete the information model from the repository, it is no longer available in the development system for use in the CODESYS Development System. |
|
“Details” |
Opens the “Details” dialog for the selected information model. The dialog includes additional information about the information model. In “Alias”, you can specify an alias name for the URI. Moreover, information is displayed as to whether or not a documentation for the information model is available.
|
|
“Documentation” |
Opens the installed documentation for the selected information model. If no documentation is installed for the selected information model, then the command is disabled. |
|
“Display all versions” |
All installed versions of the information model are displayed in a tree structure. |