Symbol: 
Function: The command loads a recipe from a file.
Call: Menu bar: “Recipes”.
Requirement: You have selected a field in the recipe column of a recipe definition.
This command overwrites the values of the selected recipe of the recipe definition.
If you have selected the option “Recipe Management in the PLC”, please note the following.
If you change recipes in the project by choosing the command “Load Recipe” or “Read Recipe”, then an online change is required when logging in again.
If you want to overwrite only individual recipe variables with new values, then remove the values for the other variables before loading to the recipe file. Entries without value definitions are not read, and therefore updating leaves these variables unchanged on the PLC and in the project.
For values of the data type REAL/LREAL, the hexadecimal value is also written to the recipe file in some cases. This is necessary so that the exact identical value is restored when converting back. In this case, change the decimal value and delete the hexadecimal value.