Symbol: 
Function: This command loads a recipe from a file and writes the values to the variables in the PLC.
Call: Menu bar: “Recipes”.
Requirement: The application is in online mode. You have selected the value of a recipe in the recipe definition.
After choosing the command, you are prompted either to write the variable values also to the recipe in the project or only to write them to the PLC. Updating the values in the recipe could require an online change when logging in again.
When you choose this command, CODESYS overwrites the values of the selected recipe of the recipe definition. In addition, these recipe values overwrite the variable values in the PLC.
If you want to overwrite only individual recipe variables with new values, then remove the values for the other variables before loading to the recipe file. Entries without value definitions are not read, and therefore updating leaves these variables unchanged on the PLC and in the project.
For values of the data type REAL/LREAL, the hexadecimal value is also written to the recipe file in some cases. This is necessary so that the exact identical value is restored when converting back. In this case, change the decimal value and delete the hexadecimal value.