Symbol
Function: This command inserts a new line for a variable declaration in the declaration editor and the input field for the variable name opens.
Call: Context menu in the tabular declaration editor; button in the declaration heading.
To edit the other fields of the declaration lines, double-click the fields and select the data from the drop-down lists or by means of the respective dialogs.
See also