Function: This command opens a dialog box for importing objects from an XML file.
Call: Menu “Project”
Requirement: A project is open.
Dialog box 'Import'
The dialog box lists all objects from the export file that CODESYS can import at this point.
“Currently selected target objects” |
Object that is selected in the Device tree |
“Insertable items” |
Displays all objects of the export file that CODESYS can insert below the selected object. |
“Show contents” |
Displays the contents of the export file in a tree structure |